• My Account
  • 0
Resources / Application Notes / Optics / Advantages of Using Plastic Hybrid Aspheric Lenses
Advantages of Using Plastic Hybrid Aspheric Lenses
Edmund Optics Inc.

Advantages of Using Plastic Hybrid Aspheric Lenses

Aberrations | Equations | Benefits | Selection Guide

plastic hybrid aspheric lens

TECHSPEC® Plastic Hybrid Aspheric Lenses are low cost optical components that lack both spherical and chromatic aberrations. These aspheric lenses provide optical designers with unique, single element solutions for achieving diffraction-limited focusing performance at high numerical apertures with broadband light sources. These aspheric lenses consist of a diffractive surface that has been added to a molded aspheric lens. The aspheric lens eliminates all spherical aberration, while the diffractive surface has a net effect of introducing negative dispersion – when properly tuned to the refractive index and wavelength design of the lens, chromatic aberration is eliminated as well.

Spherical and Chromatic Aberrations

There are two major forms of axial optical aberrations inherent in common optical lenses: spherical aberration and chromatic aberration. Spherical aberration is an inherent characteristic of any lens whose surface is a section of a sphere. Light originating from the same object point comes to a focus at slightly different points (P and P’), depending on whether the rays pass through the center of the lens or the periphery (Figure 1).

Spherical Aberration in a Single Positive Lens
Figure 1: Spherical Aberration in a Single Positive Lens
Transverse Chromatic Aberration of a Single Positive Lens
Figure 2.1: Transverse Chromatic Aberration of a Single Positive Lens
Longitudinal Chromatic Aberration of a Single Positive Lens
Figure 2.2: Longitudinal Chromatic Aberration of a Single Positive Lens

Chromatic aberration results from material dispersion. Because different colors of light refract by different amounts, an image point formed by light of one color does not coincide with the corresponding image point formed by light of a different color (Figures 2.1 and 2.2).

Important Equations

Spherical aberration is typically eliminated by substituting an aspherical surface for the more common spherical surface. The surface profile (sag) is given by Equation 1:

Equation 1 (1)

Where
Z = sag of surface parallel to the optical axis
s = radial distance from the optical axis
C = curvature, inverse of radius
k = conic constant
A4, A6, A8 = 4th, 6th, 8th… order aspheric terms

However, this does not correct chromatic aberration. Therefore, for a monochromatic light source, the aspheric surface will provide diffraction limited focusing at a single wavelength, but will suffer a large spot size over a broader wavelength.

A diffractive surface will correct the spherical aberration, as shown in Equation 2.

Equation 2 (2)

Where
Y = radial position from center of lens (for instance, if 0 is the center of the lens, 12.5mm will be the edge of a 25mm diameter lens, etc.)
nd = index of refraction of the material at 587.6nm
Step Height = λ/nd-1
λ = the wavelength of interest

By combining the two features onto a single element, a component that eliminates both chromatic and spherical aberration is created. That surface is described simply as the sum of the Zasph and Zdiff coefficients.

For tips on modeling diffractives in Zemax and Code V, visit the Optics Realm blog.

Customer Benefits

Optical designers often need to focus light at very short distances, or collect and collimate as much light as possible from very divergent light sources. Basic optical principles dictate that a high numerical aperture optical lens is required for either of these scenarios. A high numerical aperture optical lens will typically have a focal length equal to or shorter than the clear aperture of the optical system, allowing the designer to maintain as compact of an optical train as possible.

For example, an optical designer has multiple options for achieving a focal length that is equal to his clear aperture (a scenario known as an F/1 lens, or a lens with a numerical aperture of 0.50). The simplest option is to use a standard plano-convex lens, available from a number of distributors. Spot diagram, chromatic focal shift graph, polychromatic diffraction MTF, and transverse ray fan plot for the wavelength range of 486 - 656nm are provided for #45-097 25mm Diameter x 25mm FL PCX lens.

PCX Lens

Spot Diagram for #45-097 25mm Dia. x 25mm FL PCX Lens
Figure 3.1: Spot Diagram for #45-097 25mm Dia. x 25mm FL PCX Lens
Chromatic Focal Shift Graph for #45-097 25mm Dia. x 25mm FL PCX Lens
Figure 3.2: Chromatic Focal Shift Graph for #45-097 25mm Dia. x 25mm FL PCX Lens
Polychromatic Diffraction MTF Graph for #45-097 25mm Dia. x 25mm FL PCX Lens
Figure 3.3: Polychromatic Diffraction MTF Graph for #45-097 25mm Dia. x 25mm FL PCX Lens
Transverse Ray Fan Plot for #45-097 25mm Dia. x 25mm FL PCX Lens
Figure 3.4: Transverse Ray Fan Plot for #45-097 25mm Dia. x 25mm FL PCX Lens

For improved performance, the optical designer could consider an achromatic lens of the same form factor, for example #65-553 25mm Diameter x 25mm Focal Length Achromatic Lens. Again, the same characteristics are shown over the same wavelength range. A 74% decrease in spot size with a 73% decrease in chromatic focal shift can be seen, yielding an MTF of 13 lp/mm at 40% contrast, a substantial gain versus the aforementioned singlet lens.

Spot Diagram for #65-553 25mm Dia. x 25mm FL Achromatic Lens
Figure 4.1: pot Diagram for #65-553 25mm Dia. x 25mm FL Achromatic Lens
Chromatic Focal Shift Graph for #65-553 25mm Dia. x 25mm FL Achromatic Lens
Figure 4.2: Chromatic Focal Shift Graph for #65-553 25mm Dia. x 25mm FL Achromatic Lens
Polychromatic Diffraction MTF Graph for #65-553 25mm Dia. x 25mm FL Achromatic Lens
Figure 4.3: Polychromatic Diffraction MTF Graph for #65-553 25mm Dia. x 25mm FL Achromatic Lens
Transverse Ray Fan Plot for #65-553 25mm Dia. x 25mm FL Achromatic Lens
Figure 4.4: Transverse Ray Fan Plot for #65-553 25mm Dia. x 25mm FL Achromatic Lens

For maximum performance, the optical designer should choose a plastic hybrid aspheric lens. In this scenario, the exact same form factor and wavelength range are used, this time with #65-992 25mm Diameter x 25mm FL Hybrid Aspheric Lens. As shown, this lens provides diffraction limited focusing performance, yielding the optimum performance for the designer.

Plastic Hybrid Lens

Spot Diagram for #65-992 25mm Dia. x 25mm FL Hybrid Aspheric Lens
Figure 5.1: Spot Diagram for #65-992 25mm Dia. x 25mm FL Hybrid Aspheric Lens
Chromatic Focal Shift Graph for #65-992 25mm Dia. x 25mm FL Hybrid Aspheric Lens
Figure 5.2: Chromatic Focal Shift Graph for #65-992 25mm Dia. x 25mm FL Hybrid Aspheric Lens
Polychromatic Diffraction MTF Graph for #65-992 25mm Dia. x 25mm FL Hybrid Aspheric Lens
Figure 5.3: Polychromatic Diffraction MTF Graph for #65-992 25mm Dia. x 25mm FL Hybrid Aspheric Lens
Transverse Ray Fan Plot for #65-992 25mm Dia. x 25mm FL Hybrid Aspheric Lens
Figure 5.4: Transverse Ray Fan Plot for #65-992 25mm Dia. x 25mm FL Hybrid Aspheric Lens

Comparing the spot diagrams, chromatic focal shift graphs, polychromatic diffraction MTFs, and transverse ray fan plots of a plano-convex (PCX) lens, achromatic lens, and hybrid aspheric lens, it is easy to see the advantages of using plastic hybrid aspheric lenses for achieving diffraction-limited focusing performance at high numerical apertures with broadband light sources.

Selection Guide

Edmund Optics® TECHSPEC® Plastic Aspheres and TECHSPEC® Plastic Hybrid Aspheres families are both manufactured utilizing Zeon Chemical’s Zeonex E48R material. Zeonex materials feature high transparency, low fluorescence, low birefrengence, low water absorption, and high heat and chemical resistance, making it a superior material vs. other commonly available plastics. Zeonex is a Cylco Olefin Polymer (COP) material.

Plastic Materials Selection Guide
Property Glass Zeonex E48R PMMA Polycarbonate Polystyrene Arton®
Transmission Excellent Excellent Excellent Good Very Good Excellent
Low Refractive Index Excellent Excellent Excellent Poor Poor Good
Low Birefringence Excellent Excellent Excellent Poor Poor Excellent
Low Water Absorption Excellent Excellent Poor Good Excellent Excellent
Impact Resistance Poor Good Good Excellent Good Excellent
Moldability Fair Excellent Good Excellent Excellent Good
Heat Resistance Excellent Good Poor Good Poor Very Good
Coating Adhesion Excellent Good Fair Fair Fair Good

Learn all about the anatomy, benefits, and manufacturing of aspheric lenses before determining what type of asphere is right for your application

Offered uncoated or with multiple anti-reflection coating options for the UV, visible, or IR spectrum. Optical glass, crystalline, plastic, polished, or molded versions available. Buy Now!

Hundreds of stock aspheric lenses ready for purchase, available in glass, plastic, or infrared crystalline material. Don’t see what you need? We can make it.

Need to contact Edmund Optics? Use any of our fast and friendly services to meet your needs.

Need a Quote?

Edmund Optics Facebook Edmund Optics Twitter Edmund Optics YouTube Edmund Optics LinkedIn Edmund Optics Google+ Edmund Optics Instagram