LCD Monitors

×
  • Multiple Sizes
  • Cost Effective
  • Fast Response Time

LCD monitors are very popular because of their great space saving advantages as opposed to the bulky shape of a CRT monitor. The monitor's can be connected to any of our color or monochrome analog CCD cameras via connecting video cable.

All input connections on the 15.1" monitor are accessible via a removable back panel. One of the many OSD (on screen display) features of the 15.1" monitor is an automatic adjustment function that adjusts the size, position, and phase optimally according to the applied video signal. Power supply and tip/tilt mount included.