Provide Feedback

We continuously listen to and incorporate customer feedback and suggestions to improve the EO website. Is there something you liked or disliked? Please take a minute and let us know! If you leave contact information, we’ll be sure to respond.

Need Help?

Are you looking for technical support or have a sales-related question? Use any of our fast and friendly services to meet your needs: email sales or technical support, contact our regional offices, or chat live with us.

ATTENTION UNIVERSITIES: Deadline Extended to July 10 for Educational Award. | Apply Now!

 

Glossary

Application Notes | Articles | Tech Tools | FAQs | Glossary | Marketing Literature | Newsletter | Video Resources

A B C D E F G H I J K L M N O P Q R S T U V W X Y Z

Neutral Density Filter (ND)

A type of filter that yields a constant attenuation, or optical density, value over a range of wavelengths (i.e. spectrally flat). It is useful for attenuating, or reducing, the amount of light in a system.

See also Filter, Continuously Variable Apodizing Filter, Optical Density (OD)

NIR (Near Infrared)

The portion of the electromagnetic spectrum from 700 to 1100nm. Definition may differ by application.

Noise

Caused by the unwanted spontaneous emission of light from a laser medium resulting in reduced optical performance.

See also Noise Equivalent Power (NEP)

Noise Equivalent Power (NEP)

The incident light power required to produce a signal on a detector that is equal to the noise. In this case, the signal-to-noise ratio is equal to one.

See also Detectivity, Noise, Signal-to-Noise Ratio (SNR)

Non-Polarizing Beamsplitter

A type of beamsplitter that splits the incident light by a specific percentage without altering the polarization state of the transmitted or reflected light.

See also Polarization, Beamsplitter

Normal Load Capacity

The maximum downward (compression) load or force that can be applied to a mechanical component perpendicular to the mounting surface. The center of force, or the center of gravity, of the load must be located in the center of the mounting surface.

See also Inverted Load Capacity, Moment Load

Notch Filter

A type of filter designed to block a pre-selected bandwidth while transmitting all other wavelengths within the design range of the filter. Manufactured using the dielectric stack method which involves using a series of thin layers of dielectric materials, of alternating refractive index.

See also Filter, Bandwidth, Dielectric Coating, Rugate Notch Filter

Nth Order

Multiple combinations of wavelength and integer order values that will satisfy any given groove spacing, angle of incidence, and diffracted angle calculated from the grating equation. Gratings are generally specified in terms of first order diffraction since efficiency decreases with higher orders.

Numerical Aperture (NA)

The sine of the vertex angle of the largest cone of meridional rays that can enter or exit an optical system. In other words, it governs the amount of light entering or exiting a system. It is inversely related to the f/#.

Nyquist Limit

The theoretical limit of a camera's resolution or sampling ability, defined as the inverse of twice the pixel size.

See also Pixel