Provide Feedback

We continuously listen to and incorporate customer feedback and suggestions to improve the EO website. Is there something you liked or disliked? Please take a minute and let us know! If you leave contact information, we’ll be sure to respond.

Need Help?

Are you looking for technical support or have a sales-related question? Use any of our fast and friendly services to meet your needs: email sales or technical support, contact our regional offices, or chat live with us.

ATTENTION UNIVERSITIES: Final Weeks to Apply for Educational Award – up to $10,000 in FREE Products. | Apply Now!

 

Glossary

Application Notes | Articles | Tech Tools | FAQs | Glossary | Marketing Literature | Newsletter | Video Resources

A B C D E F G H I J K L M N O P Q R S T U V W X Y Z

Half-Wave Optical Thickness (HWOT)

The layer of optical coating that is equal in optical thickness to one half the design wavelength. No change in reflectance/transmittance results from layers of this thickness.

See also Quarter Wave Optical Thickness (QWOT)

Heat Absorbing Glass

A type of glass filter that absorbs, rather than reflects, energy associated with heat.

See also Filter

Helical Gear

A gear with angled teeth used in helicoid movement components. It is superior to a rack and pinion because of the smoothness of operation due to tightness of the mesh between gear and rack.

See also Rack and Pinion

Helium Neon (HeNe) Laser

One of the most common types of lasers, the HeNe laser uses a combination of helium and neon gas as its laser medium. Although the most common output wavelength is 632.8nm, HeNe lasers are available in several different wavelengths.

See also Gas Laser, Argon-Ion Laser

Holographic Grating

A type of grating in which a sinusoidal "blaze" pattern is generated on the surface by exposing the grating (covered with photoresist) to an interference pattern. The sinusoidal variations in the interference pattern lead to the groove profile for the holographic element.

See also Diffraction Grating, Grating Equation, Groove Density, Ruled Grating, Relative Efficiency

Horizontal Resolution

In analog imaging, the number of individual pixels that can be distinguished in a horizontal scanning line. Expressed in terms of TV lines.

Hot Mirror

A mirror-like filter which reflects infrared light while transmitting visible light. See also Cold Mirror.

See also Cold Mirror, Filter, Dielectric Coating

Huygenian Eyepiece

An eyepiece having two plano-convex lenses of the same glass separated by half the sum of their focal lengths. This eyepiece is free of lateral chromatic aberration, but is not suitable for use with reticles.

See also Kellner Eyepiece, Periplan Eyepiece, Wide-Field Eyepiece

Hybrid Molding

A type of manufacturing technique that starts with a standard spherical surface, such as an achromatic lens, which is pressed onto a thin layer of photopolymer in an aspheric mold to create an aspheric surface. After the surfaces are compressed and UV cured at room temperature, the end result is an aspherized achromatic lens that has chromatic and spherical aberration correction properties.

See also Aspheric Lens, Achromatic Lens

Hyperfocal Distance

The (usually long) working distance beyond which all objects are at an acceptable focus. See also Depth of Field.