Need Help?

Our team is ready to assist you!


Why Use an Achromatic Lens?

Anatomy of an Achromatic Lens

An achromatic lens, also referred to as an achromat, typically consists of two optical components cemented together, usually a positive low-index (crown) element and a negative high-index (flint) element. In comparison to a singlet lens, or singlet for short, which only consists of a single piece of glass, the additional design freedom provided by using a doublet design allows for further optimization of performance. Therefore, an achromatic lens will have noticeable advantages over a comparable diameter and focal length singlet.

An achromatic lens comes in a variety of configurations, most notably, positive, negative, triplet and aspherized. It is important to note that it can be a doublet (two elements) or triplet (three elements); the number of elements is not related to the number of rays for which it corrects. In other words, an achromatic lens corrects for red and blue, independent of it being a doublet or triplet configuration. Refer to Figures 1 — 4 for illustrations of each type.

Figure 1

Figure 1: Positive [View Larger Image]

Smoothening Stage

Figure 2: Negative [View Larger Image]


Polishing Stage

Figure 3 [View Larger Image]

Chamfering Stage

Figure 4 [View Larger Image]


Legend for Configurations
Dia. Diameter R Radius of Curvature ET Edge Thickness
EFL Effective Focal Length CT Center Thickness P Principle Point
BFL Back Focal Length
  1 , 2 , 3 | Next View All

Optics Application Examples – Read our most popular Optics app note. Learn about detector systems, selecting the right lens, and building a projection system.

Laser Spot Size Calculator – Use our featured EO Tech Tool to determine spot size from user-supplied working distances.

Spotlight on EO – What's new in the tech library? With new content every month, check back often for the latest updates.