Need Help?

Our team is ready to assist you!


Optical Glass

Optical Glass Specifications

Selecting a glass material is important since different glass types have different characteristics. Edmund Optics® offers a wide variety of glass types which can be selected on the basis of the following characteristics.

The index of refraction and Abbe number of a glass are typically used by designers as degrees of freedom when designing systems. The index of refraction refers to the ratio of the speed of light in a vacuum to the speed of light through a given material at a given wavelength, while the Abbe number of a material quantifies the amount of dispersion (variations in index) for a specific spectral range. For instance, a higher index of refraction generally bends light more efficiently so there is less of a need of curvature in the lens. Spherical aberration is less present in lenses with higher indices of refraction, while light travels faster through materials with lower indices of refraction. A high Abbe number generally gives less color dispersion and reduces color aberration. Also, certain glass types have different transmission wavelength regions.

The density of a glass helps determine the weight of the optical assembly and, along with lens diameter, becomes critical for weight sensitive applications. Density also generally denotes the ability to work with the glass and is somewhat proportional to the cost of the material. When dealing with applications involving extreme temperatures and quick temperature differentials, a glass' coefficient of expansion becomes a key factor. Opto-mechanical designers need to keep this in mind when designing optical assemblies.

Many glass manufacturers offer the same material characteristics under different trade names and most have modified their products and processes to be ECO-friendly (free of lead and arsenic).

The table below shows essential values for all types of glasses.

 
Glass Name Index of Refraction (nd) Abbe Number (vd) Density (g/cm3) Coefficient of Linear Expansion* Max Operating Temp (°C)
CaF2 1.434 95.10 3.18 18.85 800
Fused Silica 1.458 67.70 2.20 0.55 1000
Schott BOROFLOAT™ 1.472 65.70 2.20 3.25 450
Corning Pyrex 7740® 1.474† 65.40† 2.23 3.20 490
S-FSL5 1.487 70.20 2.46 9.00 457
N-BK7 1.517 64.20 2.46 7.10 557
N-K5 1.522 59.50 2.59 8.20 546
B270/S1 1.523 58.50 2.55 8.20 533
Schott Zerodur® 1.542 56.20 2.53 0.05 600
N-SK11 1.564 60.80 3.08 6.50 604
N-BaK4 1.569 56.10 3.10 7.00 555
N-BaK1 1.573 57.55 3.19 7.60 592
L-BAL35 1.589 61.15 2.82 6.60 489
N-SK14 1.603 60.60 3.44 7.30 649
N-SSK8 1.618 49.80 3.33 7.10 598
N-F2 1.620 36.40 3.61 8.20 432
BaSF1 1.626 38.96 3.66 8.50 493
N-SF2 1.648 33.90 3.86 8.40 441
N-LaK22 1.651 55.89 3.73 6.60 689
S-BaH11 1.667 48.30 3.76 6.80 575
N-BaF10 1.670 47.20 3.76 6.80 580
N-SF5 1.673 32.30 4.07 8.20 425
N-SF8 1.689 31.20 4.22 8.20 422
N-LaK14 1.697 55.41 3.63 5.50 661
N-SF15 1.699 30.20 2.92 8.04 580
N-BaSF64 1.704 39.38 3.20 9.28 582
N-LaK8 1.713 53.83 3.75 5.60 643
N-SF18 1.722 29.30 4.49 8.10 422
N-SF10 1.728 28.40 4.28 7.50 454
S-TIH13 1.741 27.80 3.10 8.30 573
N-SF14 1.762 26.50 4.54 6.60 478
Sapphire** 1.768 72.20 3.97 5.30 2000
N-SF11 1.785 25.80 5.41 6.20 503
N-SF56 1.785 26.10 3.28 8.70 592
N-LaSF44 1.803 46.40 4.46 6.20 666
N-SF6 1.805 25.39 3.37 9.00 605
N-SF57 1.847 23.80 5.51 8.30 414
N-LaSF9 1.850 32.20 4.44 7.40 698
N-SF66 1.923 20.88 4.00 5.90 710
S-LAH79 2.003 28.30 5.23 6.00 699
ZnSe 2.403 N/A 5.27 7.10 250
Silicon 3.422 N/A 2.33 2.55 1500
Germanium 4.003 N/A 5.33 6.10 100

*microns/m°C (-30 to 70°C)
**Sapphire is a birefringent material. All specifications correspond to parallel to C-Axis.
†Pyrex 7740® nd and vd specified at 589.3nm

  1 , 2 | Next View All

Related Products

Optics Application Examples – Read our most popular Optics app note. Learn about detector systems, selecting the right lens, and building a projection system.

Laser Spot Size Calculator – Use our featured EO Tech Tool to determine spot size from user-supplied working distances.

Spotlight on EO – What's new in the tech library? With new content every month, check back often for the latest updates.