Need Help?

Our team is ready to assist you!


Electronic Imaging Resource Guide

The following pages in our application notes offer detailed explanations of how to select imaging components and how to help integrate them into your specific application. Our examples are based on real life situations that our customers have encountered, and then consulted us for solutions. Using these examples, we can all learn more about using imaging as a real-world solution.

These notes are divided into sections based on the fundamentals of imaging systems. Throughout the Machine Vision section of our Online Catalog there are references to these pages for additional information on how the lens works and/or how it has been tested.

We hope you find this reference useful and we welcome any feedback or any additional application examples you would like to share.


Section 1: Fundamental Parameters of an Imaging System

Field of View (FOV): The viewable area of the object under inspection. In other words, this is the portion of the object that fills the camera's sensor.

Working Distance (WD): The distance from the front of the lens to the object under inspection.

Resolution: The minimum feature size of the object that can be distinguished by the imaging system (more in-depth discussion in Sect. 2.1)

Depth of Field (DOF): The maximum object depth that can be maintained entirely in focus. DOF is also the amount of object movement (in and out of best focus) allowable while maintaining a desired amount of focus (more in-depth discussion in Sect. 2.2).

Sensor Size: The size of a camera sensor's active area, typically specified in the horizontal dimension. This parameter is important in determining the proper lens magnification required to obtain a desired field of view. The primary magnification (PMAG) of the lens is defined as the ratio between the sensor size and the FOV. Although sensor size and field of view are fundamental parameters, it is important to realize that PMAG is not.

    Sensor Size (mm)
PMAG
=
Field of View (mm)

Note: typically, only horizontal values are used.

Figure 1: Illustration of
fundamental parameters of an
imaging system.

Figure 2: Illustration of primary
magnification and the relationship between
sensor size and FOV

  1 , 2 , 3 , 4 , 5 , 6 | Next View All

Optics Application Examples – Read our most popular Optics app note. Learn about detector systems, selecting the right lens, and building a projection system.

Laser Spot Size Calculator – Use our featured EO Tech Tool to determine spot size from user-supplied working distances.

Spotlight on EO – What's new in the tech library? With new content every month, check back often for the latest updates.