Provide Feedback

We continuously listen to and incorporate customer feedback and suggestions to improve the EO website. Is there something you liked or disliked? Please take a minute and let us know! If you leave contact information, we’ll be sure to respond.

Need Help?

Are you looking for technical support or have a sales-related question? Use any of our fast and friendly services to meet your needs: email sales or technical support, contact our regional offices, or chat live with us.

Edu Award Meet Our 2015 Norman Edmund Inspiration Award Winner! | Learn More

Understanding Spatial Filters

Understanding Spatial Filters
Edmund Optics Inc.

Spatial Filters are designed to be used with lasers to "clean up" the beam. Often times a laser system does not produce a beam with a smooth intensity profile. In order to produce a clean Gaussian beam, a spatial filter is used to remove the unwanted multiple-order energy peaks and pass only the central maximum of the diffraction pattern (see illustration). Also, when a laser beam passes through a system, dust in the air or on optical components can disrupt the beam and create scattered light. This scattered light can leave unwanted ring patterns in the beam profile. The spatial filter removes this additional spatial noise from the system. The spatial filter assembly consists of a microscope objective, a pinhole aperture, and a positioning mechanism. The positioning mechanism has precision X-Y movements that center the pinhole at the focal point of the objective lens. Our TECHSPEC® Laser Objectives are designed for HeNe lasers (632.8nm) and provide the smallest spot sizes possible. Choosing the correct pinhole and objective combination will yield optimal results. The following equations were used to determine the values for the Aperture Selection Chart.

Equation 1.0 Beam Spot Diameter (microns) = (1.27 * λ * f) / D
λ = wavelength of laser (microns)
f = focal length of objective lens (mm)
D = input beam diameter (mm)
Equation 2.0 Pinhole size is then determined for the table (see note):
Pinhole Diameter (microns) = 1.5 * Beam Spot Size Diameter (microns)

Note: The factor of 1.5 in Equation 2.0 is determined as the optimal factor in order to pass the maximum amount of energy, while eliminating as much spatial noise as possible.

Aperture Selection Chart
EFL of Microscope Objective Lens (mm) 5.5mm 8.0mm 8.5mm 9.0mm
0.96mm Input Beam Dia. 8μm 10μm 12.5μm 12.5μm
0.81mm Input Beam Dia. 8μm 12.5μm 12.5μm 15μm
0.75mm Input Beam Dia. 8μm 12.5μm 15μm 15μm
0.70mm Input Beam Dia. 10μm 15μm 15μm 15μm
0.68mm Input Beam Dia. 10μm 15μm 15μm 15μm
0.63mm Input Beam Dia. 10μm 15μm 15μm 15μm
0.48mm Input Beam Dia. 12.5μm 20μm 20μm 25μm

If you would like to see other topics covered or more detailed information, let us know. We invite you to discuss any suggestions or specific application requirements with our engineering department at 800-363-1992 or contacting us online.

Bookmark and Share

Optics Application Examples – Read our most popular Optics app note. Learn about detector systems, selecting the right lens, and building a projection system.

Laser Spot Size Calculator – Use our featured EO Tech Tool to determine spot size from user-supplied working distances.

EO Imaging Lab

EO Imaging Lab – Free training videos with imaging and illumination tips and tricks.

Prescription Request Form – TECHSPEC® Lenses are available for authorized optical designers.