Our team is ready to assist you!
Application Notes | Articles | EO Tech Tools | FAQs | Glossary | Marketing Literature | Newsletter | Video Resources
A B C D E F G H I J K L M N O P Q R S T U V W X Y Z
A type of drive mechanism for rotary stages in which angular rotation is controlled by three knobs. The release knob disengages the shaft from the drive, freeing the stage to be rotated by hand to a desired location. The release knob is then tightened to re-engage the drive mechanism and transfer control to the adjustment knob which, when rotated, produces precise angular positioning of the shaft and stage top.
A type of imaging lens in which the exit pupil is located at infinity. As a result, within a certain range of working distances there is no viewing angle error or magnification error associated with features in the image that are at different heights or angles.
See also Magnification
Glass that is heat treated after fabrication in order to make it more durable and resistant to heat and thermal shock. Since heat absorbing filters are placed in front of intense light sources, they are typically tempered to increase their resistance to breaking.
The minimum driving current corresponding to lasing threshold at a specified temperature.
See also Dark Current
Determines the light collecting efficiency of a lens or optical system. High throughput means high transmitted intensity while low throughput means low transmitted intensity.
For ball bearing stages, the maximum force or load that can be applied in the direction of travel without damage to positioning stage components. The mounting surface (stage carriage) is pressed against the drive mechanism by means of a spring. As a result, the maximum thrust which the stage assembly can maintain is different when pressing towards the spring versus away from it. When pressing towards the spring, the force is taken up by the drive mechanism (i.e. micrometer). While pulling away, the force is being held in place by the spring. It is specified as Ta and Tb: Ta refers to the load capacity against the micrometer and Tb is the spring load capacity.
See also Ball Bearing Slide, Ball Bearing Stage
A type of line scanning where multiple linear arrays are placed side by side. After the first array is exposed, the charge is transferred to the neighboring line. When the object moves the distance of the separation between lines, a second exposure is taken on top of the first, and so on. Thus, each line of the object is imaged repeatedly, and the exposures are added to each other.
In terms of mechanical components, it is a mounting thread denoted by M42 x 0.75mm. T-mount components have a 42mm diameter screw thread and a 0.75mm thread pitch; the outer diameter is 48mm. In terms of imaging, it is commonly called a T2 thread or simply denoted by M42 x 0.75mm. The flange distance varies.
See also CS-Mount, C-Mount, S-Mount, F-Mount
The reflection that occurs within a material because the angle of incidence of light striking the boundary surface is in excess of the critical angle.
The temperature at which glass changes from brittle to viscous-liquid due to thermal stress. Within a well-defined operating temperature, glass does not undergo major changes to its mechanical structure; however, after a specific transformation temperature, it will deform to the point where its original optical properties no longer apply.
Refers to a common digital logic family of devices used for control in most modern electronics. TTL signals have two distinct states; "low" and "high." A logic "low" corresponds to a maximum voltage threshold of 0.8V; a "high" corresponds to a voltage greater than 2.5V.
The amount of radiant energy that passes through a medium; energy that is not reflected or absorbed.
See also Reflection
A type of chromatic aberration where the size of the image changes with wavelength. In other words, when white light is used, red, yellow, and blue wavelengths focus at separate points in a vertical plane.
See also Longitudinal Chromatic Aberration (LCA), Aberration, Chromatic Focal Shift, Lateral Color
Also known as a Corner Cube Retroreflector, it has three total internal reflections that reflect incident light back onto itself (to the accuracy specified), regardless of the direction the beam is coming from or the tilt of the prism.
See also Retroreflector
A visual device, such as a stereo scope or microscope, that incorporates two eyepiece ports and a vertical third port for alternative image pickup.
A lens with three optical components such as steinheil triplet or hastings triplet lens.
Optics Application Examples – Read our most popular Optics app note. Learn about detector systems, selecting the right lens, and building a projection system.
Laser Spot Size Calculator – Use our featured EO Tech Tool to determine spot size from user-supplied working distances.
EO Imaging Lab – Free training videos with imaging and illumination tips and tricks.