dcsimg
survey gift card   Help us improve the EO website.   Take our 5-minute survey now!

Need Help?

Our team is ready to assist you!


Glossary

Application Notes | Articles | EO Tech Tools | FAQs | Glossary | Marketing Literature | Newsletter | Video Resources

A B C D E F G H I J K L M N O P Q R S T U V W X Y Z

Off-Set Angle

The angle at which an off-axis mirror directs and focuses incident collimated light.

See also Collimated Light

Optical Density (OD)

Describes the amount of energy that can pass through an optical material. It is directly related to the transmittance of the material, which is the ability of light to propagate through a given medium.

See also Blocking, Continuously Variable Apodizing Filter, Neutral Density Filter

Optical Fiber

A type of optic comprised of a core surrounded by a relatively thin cladding layer of lower index material. This geometry causes internal reflection of light inside the fiber and defines the maximum angles accepted by the fiber. An optical fiber emits into a cone of equal angle, not as a beam of light. Coherent fiber bundles can relay images from one end to the other; whereas, incoherent bundles are used for propogration of light alone.

See also Packing Fraction, Fiber Jacket , Ball Lens, Cladding, Buffer Material, Bend Radius, Decibel (dB), Crosstalk

Optical Flat

A precisely polished flat surface, used as a reference against which the flatness of an unknown surface may be compared.

See also Power, Interference Fringe, Surface Flatness, Reference Wavelength, Irregularity, Interferometry

Optical Invariant

A useful tool that allows optical designers to determine various values without having to completely ray trace a system. It is obtained by comparing two rays within a system at any axial point. It is constant for any two rays at every point in the system. In other words, if the invariant for a set of two rays is known, ray trace one of the rays and then scale that by the invariant to find the second.

See also Lagrange Invariant

Optical Path Difference

For a perfect optical system, the optical path, or distance, from an object point to a corresponding image point will be equal for all rays. In near-perfect systems, slight differences will exist between rays resulting in an optical path difference, usually expressed in fractions of the wavelength being analyzed.

Oscilloscope

A system in which a supplied signal causes the deflection of the electron beam in a cathode-ray tube, thus forming a visible trace on the phosphor screen of the tube, allowing for examination of signal characteristics.

See also Cathode Ray Tube

Output Power

The power measured at the exit of a laser cavity, commonly expressed as minimum output or maximum output. The class designation of a laser is based in part upon this characteristic.

Optics Application Examples – Read our most popular Optics app note. Learn about detector systems, selecting the right lens, and building a projection system.

Laser Spot Size Calculator – Use our featured EO Tech Tool to determine spot size from user-supplied working distances.

EO Imaging Lab – Free training videos with imaging and illumination tips and tricks.