Our team is ready to assist you!
Application Notes | Articles | EO Tech Tools | FAQs | Glossary | Marketing Literature | Newsletter | Video Resources
A B C D E F G H I J K L M N O P Q R S T U V W X Y Z
An imaging phenomenon that limits the accuracy of measurement to at least two pixel separations because signals impinging on the sensor may fall on a pixel or on the space between pixels. Statistically speaking, the latter case may cause a response in the pixel to the immediate left or the immediate right of the space. Due to the standard scan frequency of 60Hz, such a static image will exhibit jitter between the two pixels in question over time.
See also Pixel
Optics Application Examples – Read our most popular Optics app note. Learn about detector systems, selecting the right lens, and building a projection system.
Laser Spot Size Calculator – Use our featured EO Tech Tool to determine spot size from user-supplied working distances.
EO Imaging Lab – Free training videos with imaging and illumination tips and tricks.