Our team is ready to assist you!
Application Notes | Articles | EO Tech Tools | FAQs | Glossary | Marketing Literature | Newsletter | Video Resources
A B C D E F G H I J K L M N O P Q R S T U V W X Y Z
The layer of optical coating that is equal in optical thickness to one half the design wavelength. No change in reflectance/transmittance results from layers of this thickness.
See also Quarter Wave Optical Thickness (QWOT)
A type of glass filter that absorbs, rather than reflects, energy associated with heat.
See also Filter
A gear with angled teeth used in helicoid movement components. It is superior to a rack and pinion because of the smoothness of operation due to tightness of the mesh between gear and rack.
See also Rack and Pinion
One of the most common types of lasers, the HeNe laser uses a combination of helium and neon gas as its laser medium. Although the most common output wavelength is 632.8nm, HeNe lasers are available in several different wavelengths.
See also Argon-Ion Laser, Gas Laser
A type of grating in which a sinusoidal "blaze" pattern is generated on the surface by exposing the grating (covered with photoresist) to an interference pattern. The sinusoidal variations in the interference pattern lead to the groove profile for the holographic element.
See also Ruled Grating, Relative Efficiency, Groove Density, Grating Equation, Diffraction Grating
In analog imaging, the number of individual pixels that can be distinguished in a horizontal scanning line. Expressed in terms of TV lines.
A type of filter that contains a dielectric coating designed to reflect the infrared region of the spectrum and transmit the visible region. Ideal for applications where heat and near-infrared illumination need to be removed from the transmitted beam.
See also Cold Mirror, Dielectric Coating, Filter
An eyepiece having two plano-convex lenses of the same glass separated by half the sum of their focal lengths. This eyepiece is free of lateral chromatic aberration, but is not suitable for use with reticles.
See also Wide-Field Eyepiece, Kellner Eyepiece, Periplan Eyepiece
A type of manufacturing technique that starts with a standard spherical surface, such as an achromatic lens, which is pressed onto a thin layer of photopolymer in an aspheric mold to create an aspheric surface. After the surfaces are compressed and UV cured at room temperature, the end result is an aspherized achromatic lens that has chromatic and spherical aberration correction properties.
See also Achromatic Lens, Aspheric Lens
Optics Application Examples – Read our most popular Optics app note. Learn about detector systems, selecting the right lens, and building a projection system.
Laser Spot Size Calculator – Use our featured EO Tech Tool to determine spot size from user-supplied working distances.
EO Imaging Lab – Free training videos with imaging and illumination tips and tricks.