Our team is ready to assist you!
Application Notes | Articles | EO Tech Tools | FAQs | Glossary | Marketing Literature | Newsletter | Video Resources
A B C D E F G H I J K L M N O P Q R S T U V W X Y Z
The amount a signal increases while going through an amplifier as opposed to absorption which is the decrease in signal. Most cameras have automatic gain (autogain or AGC), and some enable the user to turn it off and set it manually.
See also Automatic Gain Control (AGC)
The exponent of the function relating output signal to input signal in video cameras and monitors. Industrial cameras naturally have a gamma of 1, that is, they are linear in response. Displays, however, can have a nonlinear response corresponding to gamma values between 2 and 3. When used together the camera may incorporate gamma correction to linearize the resulting system.
A laser using gas as the active medium. The pumping mechanism is an electric discharge, although some high-power forms employ chemical reaction or gas compression and expansion to form population inversion.
See also Argon-Ion Laser, Helium Neon (HeNe) Laser
A light beam where the electric field profile in a plane perpendicular to the beam axis can be described with a Gaussian function, possibly with an added parabolic phase profile.
Ratio of the number of teeth on mating gears (larger gear : smaller gear). For example, a ratio of 16:1 means that the smaller gear (or pinion) makes sixteen revolutions for every one revolution of the larger mating gear.
In optics, a faint second image caused by reflections within an optical component. In spectroscopy, a false image of a spectral line formed by irregularities in the ruling of a diffraction grating.
See also Spectrometer, Beamsplitter
A type of mounting component that allows for adjustable movement about two perpendicular and intersecting axes (i.e. pitch and roll). Ideal for positioning applications where the position of the center of the optic must remain stationary as it is tilted.
Point source illumination similar to directional illumination, except at a sharp angle of incidence.
See also Diffuse Illumination, Directional Illumination, Axial Illumination, Darkfield Illumination
A reference code for a specific glass type that is represented by three digits, then a slash, then another three digits. It is always present in techncial prints to indicate the specifications of the glass substrate used. The first three digits refer to the three numbers after the decimal in the glass' index of refraction. The second three digits refer to the first three significant digits in the glass' Abbe number. For instance, BK7, which has an index of refraction of 1.517 and an Abbe number of 64.2, has a glass code of 517/642.
See also Index of Refraction (n), Abbe-Number, Angle of Incidence , Angle of Reflection, Dispersion
A mechanical component that allows for precise angular adjustment of an object about a fixed point located above the center of the mounting surface.
The variation in the index of refraction of a medium as the temperature changes. This gradient index (dn/dT) can be problematic when operating in unstable environments, especially if the system is designed to operate for one value of n.
See also Index of Refraction (n)
A lens whose material refractive index varies continuously as a function of spatial coordinates in the medium.
The relationship between diffracted order, wavelength, groove spacing, and angles of incidence and diffraction. It is used to determine the diffracted angle for a given incident beam.
See also Ruled Grating, Blaze Wavelength, Holographic Grating, Groove Density, Diffraction Grating, Blaze Angle
The number of grooves per area, specified as grooves/ mm or grooves/ inch of a grating. It is used to determine the groove spacing and, with the grating equation, to obtain information about the diffracted orders and incident/ diffracted angles.
See also Ruled Grating, Holographic Grating, Relative Efficiency, Grating Equation, Diffraction Grating
A type of bevel in which the edge of an optical component is ground to remove sharp corners. Compared to a seamed edge, it is used when tighter tolerances are required.
See also Seamed Edge
Optics Application Examples – Read our most popular Optics app note. Learn about detector systems, selecting the right lens, and building a projection system.
Laser Spot Size Calculator – Use our featured EO Tech Tool to determine spot size from user-supplied working distances.
EO Imaging Lab – Free training videos with imaging and illumination tips and tricks.