Our team is ready to assist you!
Application Notes | Articles | EO Tech Tools | FAQs | Glossary | Marketing Literature | Newsletter | Video Resources
A B C D E F G H I J K L M N O P Q R S T U V W X Y Z
The distance from the front of the camera mount thread, or flange, to the camera sensor's image plane. CS-mount cameras have a 12.56mm distance, whereas, C-mount cameras a 17.526mm distance.
A mechanical measurement given as the distance between the last surface of an optical lens to its image plane.
See also Principal Plane, Effective Focal Length (EFL)
An automatic function in cameras that gives higher photometric weight to objects in the center of the field of view than to those in the periphery. It increases local contrast to help avoid silhouetting.
The amount of play (lost motion) between a set of moveable parts when changing the direction of travel.
A type of positioning component comprised of a stationary base with a mobile carriage riding on top. Two rows of hardened steel balls on both sides of the base provide the smooth, accurate, low friction sliding motion between the stationary base and the top slide.
See also Thrust Capacity, Repeatability, Ball Bearing Stage
A type of positioning component comprised of a precision linear ball slide which serves as a linear bearing and guide, and a drive mechanism which accurately moves and positions the slide top along the linear axis. They provide controlled, precise point-to-point positioning along a linear axis.
See also Ball Bearing Slide, Thrust Capacity, Repeatability, Straightness, Runout
A perfectly spherical optical component often used for improving signal coupling between fibers, emitters and detectors.
See also Optical Fiber, Sphericity
Also referred to as passband or bandpass, a wavelength range used to denote a specific part of the spectrum that passes incident energy through a filter. The first order is always at the design wavelength of the filter.
See also Filter, Cavity, Full Width at Half Maximum (FWHM), Notch Filter, Central Wavelength (CWL)
The calculated distance between two exactly opposed points on a beam at a chosen fraction of peak power (typically 1/e2). It is also defined as the diameter of a circular aperture that will pass a specified percentage (usually 90%) of the total beam energy.
See also Beam Width, Beam Divergence, Beam Expander
Causes an increase in diameter from an initially collimated source. Regarding lasers, the beam divergence of an expander is measured using the ratio of output beam diameter to input beam diameter.
See also Beam Diameter, Beam Width, Beam Expander, Divergence, Fan Angle
A component commonly used with lasers to increase the beam diameter. One advantage is that expanding a beam will decrease divergence by the expansion factor. The decreased divergence is a major advantage for long distance applications despite the initial increase in beam diameter. For example, a 1mm laser beam expanded 10X will be 10mm in diameter and will have one tenth the divergence of the original beam.
See also Beam Diameter, Beam Divergence
The angular width of a beam. With respect to a conical beam of light, it is the vertex angle of the cone. The beam width is a measure of the rate of divergence or convergence of a light beam.
See also Beam Diameter, Beam Divergence
An optical component designed to separate collimated light into a specific ratio of transmissions. Examples include a variety of cube beamsplitters and plate beamsplitters.
See also Non-Polarizing Beamsplitter, Cube Beamsplitter, Plate Beamsplitter, Pellicle Beamsplitter, Polarizing Beamsplitter, Dichroic Beamsplitter
In an optical fiber, the minimum radius the fiber can be bent before introducing damages to either the core or the cladding.
See also Cladding, Optical Fiber
A slanted edge (chamfer) ground into the side of a lens, mirror, prism, or window; it is used to prevent chipping or sharp edges.
A rim designed to hold a lens or other component. Many lasers and laser diode modules have an optional mounting bezel to allow them to accept 1"-32 TPI components such as line generators or beam expanders. Mounting Bezels can also adapt the laser for use with C-Mount Integrated Mounting Components.
In image analysis software, combining adjacent pixels into one larger pixel, resulting in increased sensitivity but lower resolution.
See also Pixel
The phenomenon of double refraction in crystalline materials. Birefringent materials have slightly different indices of refraction for light that is polarized in different orientations. They will separate incident unpolarized light into its parallel and orthogonal components.
The angle between the longer leg of the sawtooth profile of a grating and the plane of its surface (as if it were polished flat). The wavelength of peak efficiency is generally referred to as the blaze wavelength. The efficiency of a grating into a desired order can be maximized by altering the blaze angle.
See also Ruled Grating, Blaze Wavelength, Grating Equation
The wavelength of peak grating efficiency based upon the blaze angle. The maximum efficiency occurs when the incident angle from the blaze normal and diffracted rays from the blaze normal are equal (Littrow configuration). Using the grating equation, it is easy to determine the appropriate blaze angle for a specific peak efficiency (blaze wavelength) or determine the blaze wavelength from the blaze angle.
See also Grating Equation, Diffraction, Blaze Angle
The amount of light that is rejected, not passed, by a filter outside the passband. Expressed as the ratio of total energy transmitted outside the passband to the total energy transmitted within the passband. Blocking values are given over a specified wavelength range.
See also Blocking Range, Optical Density (OD), Cavity
Also referred to as stopband, a wavelength interval used to denote a spectral region of energy that is not transmitted by a filter. It is typically specified in terms of Optical Density (OD).
A type of camera not yet housed or connected to particular terminations. Ideal for OEM applications due to not having dedicated housing and mounting.
The circular line containing the center of holes about a common center in mechanical components such as bases and mounts.
Beam alignment for a laser is a mechanical specification that measures how well the optical axis coincides with the mechanical axis of the laser (usually expressed as an angle). It is often critical to know the alignment of the beam output to the mechanical housing of a laser for alignment or sighting applications.
See also Static Alignment, Pointing Accuracy
A optical device for the internal inspection of hard-to-get-at mechanical parts, such as rifle barrels, sewer pipes, oil wells, or gas mains. The long narrow tube contains a telescope system with as many relay lenses as necessary.
See also Fiberscope
The point at which the dtector begins to behave as a conductor. Operating a photodiode at or above its breakdown voltage will damage the device.
See also Photodiode, Amplifiers
In reference to optical fibers, extra material to protect the core and cladding material within the component.
See also Fiber Jacket , Cladding, Optical Fiber
Optics Application Examples – Read our most popular Optics app note. Learn about detector systems, selecting the right lens, and building a projection system.
Laser Spot Size Calculator – Use our featured EO Tech Tool to determine spot size from user-supplied working distances.
EO Imaging Lab – Free training videos with imaging and illumination tips and tricks.