Need Help?

Our team is ready to assist you!


An In-Depth Look at Axicons

Focusing of Light by an Axicon

Figure 1: Focusing of Light by an Axicon [View Larger Image]

What is an Axicon?

An Axicon is a conical prism defined by its alpha (α) and apex angles. Unlike a converging lens (e.g. a plano-convex (PCX), double-convex (DCX), or aspheric lens), which is designed to focus a light source along the optical axis, the design of an Axicon focuses a light source to a line consisting of multiple points along the optical axis (Figure 1). In doing so, a beam generated by an Axicon crosses the optical axis and forms a ring of increasing diameter over distance while maintaining a constant ring thickness. Such features closely replicate the properties of a Bessel beam, a beam comprised of rings equal in power to one another.

Bessel Beam Features of an Axicon

Unlike a Gaussian beam which deteriorates over distance, a Bessel beam is non-diffracting, maintaining an unchanged transversal distribution as it propagates. Although a true Bessel beam would require an infinite amount of energy to create, an Axicon generates a close approximation with nearly non-diffracting properties within the Axicon's depth of focus (DOF). DOF is a function of the radius of the beam entering the Axicon (R), the Axicon's index of refraction (n), and the alpha angle (α):

Equation 1(1)

As stated, the thickness of the ring (t) remains constant and is easily determined; it is equivalent to the radius of the initial beam or one half the initial beam's diameter (db):

Equation 2(2)

The diameter of the ring is proportional to distance; increasing length from lens output to image (L) will increase the diameter of the ring (dr), and decreasing distance will decrease it. As Equation 3 mathematically illustrates, the diameter of the ring is related to twice the length, the tangent of the product of the refractive index (n), and the alpha angle (α).

Equation 3(3)

Figures 2 - 3 are real-world images of the focusing of green laser light by an Axicon; the figures illustrate an Axicon's ability to maintain constant ring thickness and proportional diameter with distance. In Figure 2, the Axicon is positioned at L = 228.6mm and in Figure 3, at L = 355.6mm. The images were created using a laser with a beam diameter of 4mm, a 127mm x 127mm white balance target, and an Axicon with a 20° alpha angle. For both Figure 2 and Figure 3, the thickness of the ring remained 2mm, while the diameter increased from approximately 73.66mm at L = 228.6mm between Axicon output and image to approximately 114.3mm at L = 355.6mm.

Green Laser Light from an Axicon at L = 228.6mm

Figure 2: Green Laser Light from an Axicon at L = 228.6mm [View Larger Image]

Green Laser Light from an Axicon at L = 355.6mm

Figure 3: Green Laser Light from an Axicon at L = 355.6mm [View Larger Image]


Applications of an Axicon

The unique properties of an Axicon allow for applications in a range of research and medical fields. For example, an Axicon can aid improvements in laser corneal surgery, an outpatient corrective vision surgical procedure in which a laser ablates corneal tissue to correct the eye's refractive state. An Axicon's ability to focus a laser beam into a ring provides increased capability in smoothing and vaporizing the corneal tissue. With the use of a negative and positive Axicon, ring diameter can be adjusted to fit the patient's and surgeon's needs by manipulating the distance between the two axicons.

An Axicon is also beneficial in optical trapping, the use of a laser to create attractive and repulsive forces in order to manipulate microparticles and cells. The ring generated by an Axicon serves as a repulsive wall, trapping particles within the darker inner region of the beam, ideal for precise interaction with the trapped particle(s).

Interested in a short video on Axicons?

Interested in a short video on Axicons?

View our Axicons Review video for additional information.

Using Optical Components with an Axicon

In order to replicate a Bessel beam, an Axicon and laser must be aligned so that the laser beam travels along the Axicon's optical axis. A variety of optical components can be used to achieve the alignment and precision needed to do this including lasers, beam expanders, optical lens mounts, and posts and post holders. For example, beam expanders collimate incident laser light and reduce its divergence so that an Axicon can accurately create a ring shaped beam, and optical lens mounts securely hold the Axicon in place and can offer additional degrees of freedom for micron, or sub-micron, alignment.

By focusing a light source in a line along its optical axis, an Axicon creates an approximation of a Bessel beam. Although the ring diameter increases and decreases proportionally to the distance between the Axicon and the image, the ring thickness remains the same. Axicons are ideal for measurement and alignment, research, and medical applications requiring a ring shaped laser output.


References

  1. Mallik, Proteep. "The Axicon." 7 December 2005. PowerPoint. 15 November 2010.
  2. Haw, Weldon W. MD, and Edward E. Manche, MD. "Prospective Study of Photorefractive Keratectomy for Hyperopia Using an Axicon Lens and Erodible Mask." Journal of Refractive Surgery 16 (2000): 724-30.

Corporate Brochure – Discover our stock and custom optical capabilities.

Global Presence – Over 15 regional offices in the Americas, Europe, and Asia to offer local support with world-class service.

We Design. We Manufacture. We Deliver.

We Design. We Manufacture. We Deliver. – Spherical optics, aspheric lenses, prisms, imaging lenses, imaging and laser optics assemblies, and mechanics are just a few of our expertise.

Education Programs

Education Programs – Free optics, support, awesome videos, and amazing careers.