dcsimg
survey gift card   Help us improve the EO website.   Take our 5-minute survey now!

Need Help?

Our team is ready to assist you!


Linear Variable Filters Ideal for Fluorescence Applications
97% transmission with OD>4 blocking

Linear Variable Filters Ideal for Fluorescence Applications <br />97% transmission with OD>4 blocking

April 15, 2011, Barrington, NJ USA — Edmund Optics (EO), the premier provider of optical components, introduces its new Linear Variable Filters. These filters are designed for both individual and combined use for maximum versatility and are available in both Long-Pass and Short-Pass Options.

A single filter can replace entire filter set

Linear Variable Filters are manufactured with an interference coating that is intentionally wedged in one direction, creating a linear shift of the center wavelength across the length of the entire substrate. This linear shift allows the broad filtering capabilities that are demonstrated by the Short-Wave and Long-Wave Variable Filters. The two types of filters – Short- and Long-Wave – work inversely to one another. The Short-Wave Variable Filter passes light throughout the filter’s length until a blocking band is reached, while the Long-Wave Variable Filter blocks light until a transmission band is reached. These blocking and transmission bands may be adjusted by reorienting the filter to the light source. Using its broad blocking and transmission range, a single linear variable filter can replace an entire filter set, making them extremely economical and saving valuable space.

Filter pairs create Custom Bandpass Filters

Linear Variable Filters allow for blocking and passing of targeted wavelengths. When used independently, the Linear Variable Short-Wave Pass Filter has a wavelength range of 330-750 nm with an excellent average transmission of 97% from 400-750 nm. The Linear Variable Long-Wave Pass Filter has a wavelength range of 300-845 nm and an impressive average transmission of 97% across its entire wavelength range for maximum efficiency. The filters provide blocking of OD>4. When the Short-Pass and Long-Pass Filters are combined, they can operate as a laser-line filter or as a variable bandpass filter with a tunable center wavelength and bandwidth for a vast array of applications.

Combined filters can be used as single variable excitation filter

In order to reduce scattered light and harmonics, combined Long- and Short-Wave Linear Variable Filters may be synchronized with a single moving grade spectrometer. Combined Linear Variable Filters can also be used as a single variable excitation filter for a wide variety of fluorescence applications using white light sources. Linear Variable Filters are in-stock and available for immediate delivery for fast turnaround and excellent value.

Corporate Brochure – Discover our stock and custom optical capabilities.

Global Presence – Over 15 regional offices in the Americas, Europe, and Asia to offer local support with world-class service.

We Design. We Manufacture. We Deliver.

We Design. We Manufacture. We Deliver. – Spherical optics, aspheric lenses, prisms, imaging lenses, imaging and laser optics assemblies, and mechanics are just a few of our expertise.

Education Programs

Education Programs – Free optics, support, awesome videos, and amazing careers.

No More Alpha Characters – Due to your direct feedback we have removed the alpha characters preceding our part numbers. If your purchasing systems send orders with alpha characters, we will still process your order as normal.